Keep Cool

Keep Cool

Discover your true no.1 fan…

Keeping cool in summer has never been made so easy, with our super-efficient and portable fans offering you an effective way of cooling down; meanwhile our range of air conditioners and coolers present the perfect solution for getting rooms at work and home feeling both comfortable and cool.

Fantastic Deals

Shop by Fan Type

Some interesting questions…

Pedestal fans generally come on a height-adjustable stand and can be positioned at a height suitable to the user's requirements, while Tower fans normally have a long rectangular outlet, with the bottom part positioned closer to the floor.

Once air has been drawn into the unit, the air conditioner compresses and liquefies it before cooling the air in a condenser and allowing it to expand through an evaporator. The unit then re-circulates the air into the room in a cooler state, or at a warmer temperature if using the air conditioning unit in reverse mode. Simple!

Working in a similar way to a thermostat, a humidistat will trigger the dehumidifier to start working once humidity levels reach a certain point.

Air coolers and air conditioners will often have oscillating louvres, which move allowing the air to be directed in different directions rather than solely on a fixed point.

BTU is a unit of energy, which stands for British thermal units. One BTU relates to the amount of energy needed to raise the temperature of one pound of water by 1°F. Energy is more commonly measured in Joules with one BTU equivalent to approximately 1055 joules. Wish you'd never asked? Thought so.

It's a discrete fan designed for use at your desk, which plugs into the USB port on your PC or laptop. It takes up less room than a conventional desk fan and is a cost-effective way of keeping cool at work. You can view our selection of USB desk fans by clicking here.