RASPBERRY PI

The Raspberry Pi is a powerful credit-card sized micro-computer that can do anything a desktop computer can do. The board was designed to help both kids and adults learn how to programme and get started in the world of computers, all at an affordable price, making the Raspberry Pi a fantastic tool for coding in languages such as Python and Scratch. The single-board computer comes with built-in ports allowing it to interact with the outside world – it can accept accessories such as a keyboard, mouse, monitor or camera, as well as connect to the Internet, and more.

The Raspberry Pi lets you browse the web; take videos and photographs; play music and high-definition videos; or if you just need to work on a word-processor, it can do that too. Being Internet-connected gives the Raspberry Pi the ability to let makers create Raspberry Pi projects such as weather stations; voice assistants; game consoles – the possibilities are endless.

Raspberry Pi Boards

Comparison Chart

Raspberry Pi 3
Model A+
Raspberry Pi 3
Model B
Raspberry Pi 3
Model B+
Raspberry Pi 4
Model B
Raspberry Pi
Compute Module
Raspberry Pi
Compute Module 3+ Lite
Raspberry Pi
Compute Module 3+
Dimensions65x56mm85x56mm85x56mm85x56mm67.6x30mm67.6x31mm67.6x31mm
SoftwareLinuxLinuxLinuxLinuxLinuxLinuxLinux
ProcessorBCM2837B0BCM2837BCM2837B0BCM2711BCM2835BCM2837B0BCM2837B0
ARMv6ARM Cortex-A53ARM Cortex-A53ARM Cortex-A53ARMv8ARMv6ARM Cortex-A53ARM Cortex-A53
CPU Speed1.4GHz1.2GHz1.4GHz1.5GHz700MHz1.2GHz1.2GHz
CoresQuadQuadQuadQuadSingleQuadQuad
RAM512MB1GB1GB2GB/4GB/8GB512MB1GB1GB
StorageMicroSDMicroSDMicroSDMicroSD4GB eMMC-8GB/16GB/32GB eMMC
LAN-10/100mb Ethernet*10/100/1000mb Ethernet10/100/1000mb Ethernet---
Wireless2.4GHz/5GHz802.11 b/g/n2.4GHz/5GHz2.4GHz/5.0GHz---
Bluetooth4.2/BLE4.1/BLE4.2/BLE5.0/BLE---
GPIO Pins40404040484848
Video OutHDMI/HDMI/HDMI/2 x micro HDMIHDMI
(via EDGE connector)
HDMI
(via EDGE connector)
HDMI
(via EDGE connector)
3.5mm/DSI3.5mm/DSI3.5mm/DSI3.5mm/DSI3.5mm/DSIDSI
(via EDGE connector)
DSI
(via EDGE connector)
DSI
(via EDGE connector)
Audio OutHDMI/3.5mmHDMI/3.5mmHDMI/3.5mmHDMI/3.5mmHDMI / Composite / Analogue (via EDGE connector)HDMI / Composite / Analogue (via EDGE connector)HDMI / Composite / Analogue (via EDGE connector)
USB 2.0 Ports1442---
USB 3.0 Ports---2---
Input Voltage5V5V5V5V5V5V5V
Order CodeSC14977SC14012SC14882SC15184
SC15185
SC15613
SC13437SC15055SC15056
SC15057
SC15058

*Note: The Pi 3 B+ uses Gigabit technology but is restricted by the USB bus to a maximum of 480Mb/s.

Raspberry Pi Kits

Raspberry Pi Accessories

Explore Coding

Learn how to program in languages like Scratch and Python with the Raspberry Pi.

Raspberry Pi is capable of doing everything you’d expect a desktop computer to do, from browsing the internet and playing high-definition video, to making spreadsheets, word-processing and playing games.

Physical Computing

Raspberry Pi has the ability to interact with the outside world through a wide variety of digital projects, from home media centres and arcade gaming systems, to autonomous robots and automated irrigation systems

Product Listing from Raspberry PI


Cable, Leads & Connectors

Electronic & Electrical Components

Maker & Circuit Development

Show All Products (136)